CN0300: Power Consumption

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What is the power consumption of the ADuCM360?

 

When operating normally, the entire circuit consumes 2.25 mA typically. When
held in a reset state, the entire circuit consumes less than 600 μA.  For
further details on power consumption of the ADuCM360, see AN-1111.

http://www.analog.com/static/imported-files/application_notes/AN-1111.pdf

Attachments

    Outcomes