ADUCM360/361: Configuring unused ADC inputs

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I have some unused ADC inputs and GPIO pins that are not used in my design. 
How should I
configure these pins to minimize current consumption?

 

ADC inputs - tie these directly to ground. The leakage current on the analog
pins is low –
typically 1nA.  The digital pins have an internal pull-up to IOVDD. This
pull-up is typically 50Kohms. Because of the pull-ups, these pins can be left
unconnected. Another option is to tie them externally to IOVDD to minimize the
current flowing through the pull-up.

Attachments

    Outcomes