Configuration of current source IEXC[0|1]

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

When I use the current source IEXC[0|1] on pin 11 and 12, can I still use the
analog input on these pins?

 

THE PINS CAN BE CONFIGURED FOR ONE OF THE FOLLOWING FUNCTIONS :
P1.6/AIN7/IEXC1. You cannot configure these pins as external current soources
and analog inputs at the same time.

Attachments

    Outcomes