Which is the maximum value of the external clock  for the PWM on ADuc848?

Document created by analog-archivist Employee on Feb 23, 2016Last modified by carol.nelson on Jan 24, 2018
Version 2Show Document
  • View in full screen mode

Which is the maximum value of the external clock for the PWM on ADuc848?

 

You can safely run it at up to 12.58 MHz, which is the tested maximum speed of
the core logic.
It may well work at higher rates - but we have not tested this and so we cannot
guarantee it.
In the opinion of our microconverter applications engineers, it is quite likely
that it will work
at up to 20 MHz but any risk in doing so belongs to the user and not to Analog
Devices.

Attachments

    Outcomes