ADUC848: Is there a single device with supply range 2.7 to 5.5 V?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Do you have an ADuC848 working at supply range 2.7 to 5.5 V?

 

It is not possible to get a single  ADuC848 that runs off power supplies of  3-
5 volts. You have to order either the 3V or 5V version of the device (different
silicon). Order an ADUC848 with -5 or a -3 suffix as appropriate.

Attachments

    Outcomes