What is the maximum Source current, that port P2.5 and P2.6 can deliver?

Document created by analog-archivist Employee on Feb 23, 2016Last modified by carol.nelson on Jan 24, 2018
Version 2Show Document
  • View in full screen mode

What is the maximum Source current, that port P2.5 and P2.6 can deliver?  (Note
sink current is defined in datasheet but not source current)!

 

The ADuC847 digital outputs can source up to 80uA and still be guaranteed to
output a valid logic output level (>2.4V).

Attachments

    Outcomes