ADUC834: Does changing the PLL divider value via the CD bits in PLLCON affect the baud rate?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Does changing the PLL divider value via the CD bits in PLLCON affect the baud
rate?

 

Yes, changing the CD bits does affect the baud rate. The output of the PLL
divider is the core
clock frequency which the baud rates are obtained from. See the ADuC834
datasheet (pg 62/63)
for more details.

Attachments

    Outcomes