ADuC7061: Connecting 32Khz External Crystal

Document created by analog-archivist Employee on Feb 23, 2016Last modified by carol.nelson on Jan 24, 2018
Version 2Show Document
  • View in full screen mode

I need to connect a 32kHz crystal to the XTAL pins. In the datasheet it does
not say what what capacitance crystal is required and whether external
capacitors are needed?

 

The 32KHz crystal part used and its external capacitors C18, C19 (12 pF) are
listed in the BOM and shown on schematic for the ADuC7060 evaluation board in
the User Guide UG-029 which can be found from the evaluation board link on the
ADuC7060 product page on wwww.analog.com.

Attachments

    Outcomes