Max baudrate on ADuC7060

Document created by analog-archivist Employee on Feb 23, 2016Last modified by analog-archivist Employee on Jan 24, 2018
Version 2Show Document
  • View in full screen mode

We are evaluating the ADUC7060 and we need to know if this can handle BAUD
rates above 115200? We have tried setting the following to achieve 230400
BAUD...

DL = 0x1 
N = 796 

... but it does not work: we stripped down the code to run the TX on an
interrupt just outputting one
character consecutively. At 115200 it was OK. when scoping the TX pin, I was
not able to detect transmitting characters when setting N=796, DL=1 to try and
achieve a BAUD rate of 230400. Ideally we would like to run at 921600 / 1152000
BAUD.

Following the datasheet RevB. Page79 gives the equation to work out the N and
DL value. I see the DL value “tunes” the BAUD rate generator but setting this N
value to 1 and setting DL to 1 gives a BAUD rate of 319843BAUD. So is this the
Maximum BAUD rate achievable running from a 10MHz clock?

 

The attached file works at 230k BAUD when testing on EVAL-ADuC7060QSPZ.

Also tried in polled mode and it worked fine.
As well in polled mode we got it working at 320k baud, by writing
COMDIV0 = 0x1;
COMDIV1 = 0x00;

And not writing to COMDIV2

Did not try RX mode as you only reported issues with TX mode.

Attachments

Outcomes