On-chip flash for ADSP-BF538F and ADSP-BF539F

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

It is mentioned in the data sheet that we need to connect /AMS0 to /FCE to boot
from on-chip flash.  What should be done with the /FRESET pin?


Typical applications using the Spansion flash device externally would tie
/FRESET to the system /RESET signal.  In the case of the on-chip flash on these
devices, the Blackfin processor /RESET signal serves this purpose, and no other
circuitry is required.