ADR431BRMZ, error in package type of datasheet order guide

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I notice for ADR431BRMZ that the datasheet says the package for this part
should be an 8-pin SOIC_N, but the website says it’s an 8-pin MSOP.

 

There is a mistake in the datasheet order guide for ADR431BRMZ-R7.

The part number ADR431 B RM Z -R7  breaks down into the following format:

Generic: ADR431
Grade:   B
Package type:  RM
RoHS compliant:  Z
Reel size:  R7

The package type indicator "RM" indicates that the package is 8-lead MSOP

So therefore the order guide is incorrect as it lists the package type as
8-lead SOIC_N

A request has been made to the ADR Product line Engineer to make a correction
to the datasheet order guide at the next available opportunity.

Attachments

    Outcomes