ADP3330: max reverse voltage

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I would like to know what the max. reverse voltage is on your
ADP3330-3.3 (voltage on output if input is GND)?

 

Here are the results that you've requested concerning what the max. reverse
voltage is on
ADP3330-3.3 (voltage on output if input is GND):
Breakdown occurs when output is applied with 11V and input is grounded.  It is
not specd in the datasheet, but it has been tested in the lab with several
parts and the result seem consistent. The output follows the input, and the
part no longer works in normal condition. 

Attachments

    Outcomes