ADP2504  Issues with supplied current and current limiting

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

The ADP2504 not achieving the max 1 amp as defined in the spec.

 

The ADP2504 is designed to start-up with a maximum of 100uF, if you have
additional capacitance besides the 22uF shown on the datasheet schematics that
may result in the output voltage stuck at 80% of 5V because of the current
limit.

Attachments

    Outcomes