ADP2441 Minimum ON Time

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What is the minimum ON time of ADP2441?

 

The maximum operating frequency is limited by the minimum on-time and the
required duty cycle.  ADP2441 has minimum on time of 50ns.  Low minimum on-time
makes ADP2441 suitable for applications that require a very high step-down
ratio. For example, ADP2441 can step down supply from 24V to 1.2V at 1 MHz
frequency.

Attachments

    Outcomes