ADP2384, ADP2386 - Use of EN threshold to set input voltage UVLO

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

How to use EN threshold to set the input voltage UVLO?

 

The ADP2386 has a precision enable input with a typical rising threshold of
1.17V, which can be used to program the UVLO threshold of the input voltage. A
resistor divider from PVIN through EN to GND can set both the rising and
falling thresholds of the input voltage UVLO.
For detailed information, please refer to ADP2386 data sheet, page17,
PROGRAMMING THE INPUT VOLTAGE UVLO section.

Attachments

    Outcomes