ADP2384, ADP2386 - Treatment of GND-EP (pin 25) and SW-EP (pin 26)

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

When doing layout, how do I treat the GND-EP (pin 25) and SW-EP (pin 26)?

 

The GND exposed pad should be connected to the ground plane to reduce thermal
resistance.
Add several vias on the GND-EP to connect it to the internal ground plane.
The SW exposed pad should be connected to the SW pins of ADP2386 by using short
wide traces or copper SW plane.

Attachments

    Outcomes