ADN8834: Evaluation board difference

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

We are interested in the ADN8834.
What is the difference between ADN8834CB-EVALZ and ADN8834MB-EVALZ? Do you have
any additional information or datasheet for the eval kits?


The main difference of the two evaluation boards is the following: 
The heating and cooling current limit is fixed on ADN8834CB-EVALZ board.  The
maximum output voltage and temperature set-point are also fixed.

But on ADN8834MB-EVALZ, the PID parameters are configurable and all the
parameters above are programmable. In addition the ADN8834MB-EVALZ can not be
used alone, a CB-EVALZ must be inserted into the socket as shown in below