ADP1048 - is is possible to use the ADP1048 with higher input frequencies?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

what is the max power input frequency for the ADP1048
(more than 60Hz ?). I need 500Hz - is this possible?

 

yes - the ADP1048 kann also be used from 500Hz - 1kHz (e.g. net in an airplane)
1 person found this helpful

Attachments

    Outcomes