ADP1046 Daughter Board compatible with existing one for ADP1043

Document created by analog-archivist Employee on Feb 23, 2016Last modified by analog-archivist Employee on Feb 23, 2016
Version 2Show Document
  • View in full screen mode

Is ADP1046 Daughter Board compatible with existing one for ADP1043?

 

Please find attached to this email, a document highlighting the list of changes
between ADP1043 and ADP1046.
The ADP1046 daughter card is pin to pin compatible with the ADP1043 daughter
card. The only thing I would modify is the ACSNS circuit on the main board.
Check the attached document for the differences.

One more thing to note, is the ADP1043 settings cannot be directly loaded into
the ADP1046. You can run the two GUIs simultaneously side-by-side and replicate
the settings.
1 person found this helpful

Outcomes