ADN2882 Evaluation Board

Document created by analog-archivist Employee on Feb 23, 2016Last modified by analog-archivist Employee on Feb 23, 2016
Version 2Show Document
  • View in full screen mode

I would like to know if it is possible to connect a photodiode to the
EVAL-ADN2882-EXT evaluation board.
Is there an output SMA connector that can be connected to the input SMA
connector of another PCB containing the photodiode.

 

The EVAL-ADN2882-EXT is a one ROSA evaluation board. It should host one ADN2882
based ROSA to be one optical receiver. Customer needs to build a ROSA with a
Photodiode and ADN2882 (please refer to ADN2882 datasheet on page 9), then
mount this ROSA on this evaluation board. EVAL-ADN2882-EXT provides SAM
connectors as the ADN2882 differential outputs.

Attachments

Outcomes