ADN2817 error correction

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

My receiver signal may have some "errors" introduced due to  various factors
Can the ADN2817 be able to remove and "clean up the signal". 

Hence Can the CDR remove errors  seen on its inputs so that its output is
effectively cleaned up and thus error  free ?

 

The ADN2817 ia a Clock and Data Recovery ICs.
Its  intended operation is for data and clock recovery (i.e. decoding and
separation of data and clk). Hence where these two signal are original encode
from.

Please note there is no error correction function with this IC. It will however
it clean up and separate individually the data and clock lines.

If there are bit errror enbedded in the encoding data. This is most likey to be
propagate after CDR.

Attachments

    Outcomes