ADM696: Datasheet reset assertion guarantee

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

In the  datasheet there is a contradiction: In the first page, the penultimate
sentence reads "RESET assertion is guaranteed with VCC as low as 1 V." - On the
following page though, in the table ADM696/ADM697?SPECIFICATIONS, VCC Operating
Voltage Range is from 3.0 V to 5.5, and there is NO mention to the statement
"RESET assertion is guaranteed with VCC as low as 1 V." Please let me know
which one is true?


The device will be held in reset all the way down to 1V.  The 3.0V to 5.5V spec
refers to the normal operating range of the device (ie) where the monitoring
circuit is functioning accurately, where the timeouts on the device work
correctly.  Once you drop below the 3.0V value, there is no guarantee that
these circuits are working correctly.  However, when Vcc is at this level you
should be in reset anyway and the part is guaranteed to actively pull reset low
all the way down to Vcc = 1V.