Can I configure ADM3491 in half duplex mode of operation

Document created by analog-archivist Employee on Feb 23, 2016Last modified by analog-archivist Employee on Feb 23, 2016
Version 2Show Document
  • View in full screen mode

I want to use  the ADM3491 in full or half duplex RS485 application. This
device is for full duplex operation but if I connect A with Y and B with Z, is
it possible to work in half duplex ?

 

Yes it is possible to operate the ADM3491 in a half duplex configuration if A
is connected to Y and B is connected to Z. Figure 41 given in the ADM2582E
datasheet is a good example of where a Full Duplex RS-485 transceiver is
configured in a Half Duplex setup (figure attached)

Outcomes