S-Parameters for ADL5801 Mixer

Document created by analog-archivist Employee on Feb 23, 2016Last modified by analog-archivist Employee on Aug 10, 2016
Version 2Show Document
  • View in full screen mode

I'm developing a wideband RF measurement system employing the ADL5801 mixer and
need to optimize the RF Port input return loss for the frequency range of 1.5
to 3.0 GHz. Therefore it would be great if you could provide me with a
de-embedded S-Parameter set of the ADL5801 in Touchstone format, as the
datasheet only states the magnitude of the typical insertion loss and not the
phase or a complex impedance over frequency in a Smith-chart.

 

Please find attached the s2p file with de-embedded s-parameters for the RF port
of the ADL5801.

Attachments

Outcomes