Gain of the ADL5610/1, ADL5544/5?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Is it possible to reduce the gain of the ADL5610/1, ADL5544/5?

 

Yes. The gain of these devices can be reduced by adding a feedback path from
the RF input to the RF output. The de-embedded s parameter model file can be
used to compute the specific component values required to meet the application
requirements. A 100pF capacitor and 1kΩ resistor could be a good starting point
for a lot of applications.

Attachments

    Outcomes