In the ADL5511 datasheet, pins 6, 7, 8, 12 and 13 are designated as No Connect. Are these pins really No-Connect or can I ground them?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

In the ADL5511 datasheet, pins 6, 7, 8, 12 and 13 are designated as No Connect.
Are these pins really No-Connect or can I ground them?

 

Pins 6, 8, 12 and 13 are not internally wire-bonded to the die so it's OK to
ground these pins if you wish. However, Pin 7 is wire-bonded to the die so this
pin should not be grounded.

Attachments

    Outcomes