Phase shift a sinus RF signal in the range between 150Mhz and 450Mhz?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

In my application I need to phase-shift a sinus RF signal in the range between
150MHz and 450MHz, with an accuracy of 1degree.
Can you recommend any device?

 

It sounds that you are looking for vector modulator, which allows
amplitude/phase shifting. Please refer to below link for vector modulator and
refer attached file for quadrature modulator:
http://www.analog.com/en/products/rf-microwave/phase-shifters-vector-modulators/
vector-modulators.html

However, the ADL5390 seems like the most suitable option for the frequency
range specified.

Attachments

    Outcomes