ADL5317: Is the overcurrent protection adjustable on ADL5317?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Is the overcurrent protection adjustable on ADL5317?

 

The overcurrent protection on ADL5317 is not programmable (unlike with the
ADL5315), but the threshold current at which the devices starts to limit varies
from the stated 18mA; it may trip as low as 14 mA and as high as 21 mA.
(The ADL5315 provides a resistor-programmable input current limit with a fixed
maximum of 16 mA for the RLIM pin tied to VPOS).

Attachments

    Outcomes