ADIS16445 - Initialization sequence

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What type of initialization sequence does the ADIS16445 require?

 

While the control registers offer a number of configuration options, the
ADIS16445 requires no initialization. Once the device has +3.3V across its
VDD/GND pins, it will self-initialize and then start producing data. The
data-ready line will start pulsing when data updates begin, so it also serves
as a convenient indicator of “start-up completion.”

Attachments

    Outcomes