ADIS16445 - Definition of full calibration

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What does fully-calibrated mean?

 

For the ADIS16445, this means that each sensor has its own unique calibration
formula that improves bias and sensitivity accuracy, over temperature, by a
factor of 10-20x, when compared with un-calibrated devices. Is also means that
each sensor is electronically aligned to an orthogonal frame, which reduces
cross-axis sensitivity by greater than 20x over a typical discrete IMU design.

Attachments

    Outcomes