ADIS16405 working at a different sample rate other than default 819.2SPS

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

We have a customer looking at using the ADIS16405 in a virtual horizon
autopilot application. The default sample rate is 819.2 sps. He wants to use
the part at 1024 sps. What likely affect this will have on the performance of
the device and anything they should consider?

 

We do not have as much data for 1024SPS as we do for the 819.2SPS but the parts
should perform very close to normal.  The primary concern would be to make sure
that the clock input signal is clean (low jitter).  Out of curiosity, why do
they want to use 1024 SPS instead of the internal clock?

Attachments

    Outcomes