The noise of ADIS16364

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

For ADIS16364, If I put ADIS16364 on the table in static state, the output data
is 0.1~1.5degree/sec(test condition: measure range: +/-300), is it
well-balanced? I checked ADIS16364's datasheet, the output noise is 0.9
degree/sec, so I think 1.5 degree/sec output is normal, do you agree with me?

 

The noise you are seeing is normal.  You can lower it by using the filtering in
the Configuration/Operation menu.  The offset can be handled by using the
Precision Auto Null function inside the Calibration menu in the evaluation
software.  We have observed the overall bias shifting as high as 2-3 deg/sec
when a device is exposed to pressure, large temperature changes, etc (such as
shipping) but the Precision Auto Null takes care of that.  In this case, the
single-temp adjustment from the Precision Auto Null preserves the entire
factory calibration.

Attachments

    Outcomes