critical performance parameters

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What are the critical performance parameters?

 

For high-level discussions, here are the appropriate talking points, but keep
in mind that many customers are not going to have an idea of what they need.
While we share this information, they key message to communicate is the full
sensing and analysis capabilities, which enable quick data collection and
analysis.
• Frequency range up to 5.5kHz
• Range = ±18g, tri-axis
• Noise density = 240μg/√Hz
• 512-point real-value FFT
• Programmable FFT averages; up to 255 average cycles

Attachments

    Outcomes