ADIS16209: How do I connect pins 7,8,10,11? There are contradictions in datasheet.

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

There is some contradictory information in the ADiS16209 datasheet. While the
pin configuration (Figure 5 ) states tha pins 7,8,10,11 are DNC (Do not
connect),  figure 23 shows a schematic for the ADIS16209/PCBZ with Pins 7,8,10
and 11 grounded at J2. Meanwhile the ADiS1620x/PCBZ datasheet figure 1
schematic shows pins 7,8,10 and 11 unconnected to J2. Which is correct?

 

The figure 23 schematic in dtatasheet is incorrect. Pins 7,8,10,11 should be
not be connected to ground, These are DNC pins. Here is the correct schematic
for the ADIS16209/PCB.  The schematic in the datasheet figure 23 will be
corrected shortly.


Attachments

    Outcomes