ADG788: ESD rating

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

How much ESD can the ADG788 take? - it is not written in the datasheet.

 

For ADG788:

HBM ESD Model: 1000V
FICDM ESD Model: 1500V

ESD testing was according to FICDM and HBM model, test results for ADG788:

Field-Induced (Robotic) Charged Device Model (FICDM),Class C6, Highest Pass
Level 1500V, First Fail Level 2000V
(ESD test spec. ESD Assoc.STM5.3.1-1999)

Human Body Model (HBM) Class 1C, Highest Pass Level 1000V, First Fail Level
1500V
(ESD test spec. ESD Assoc. STM5.5.1-2001)

Attachments

    Outcomes