ADG804: Maximum voltage

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I have an application which I want to Mux between 4
Voltages(95V,98V,101V,104V), According to digital command. The average current
is 100mA, On resistance less than 1 Ohm.Can I use the ADG804?

 

Analog Devices do not have a solution for this.

The ADG804 does allow higher currents than most of our switches and
multiplexers but not high voltages !

If you refer to the Absolute Maximum ratings of the ADG804 on page 6 of the
datasheet, the maximum voltage allowed has to be within 300 milliVolts of the
power supply (Vdd).

Attachments

    Outcomes