ADG709: Life time

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Here is 2 questions about ADG709 :

(CMOS, 1.8V to 5.5V/+-2.5V, 3Ohm, Low Voltage, 4-/8-Channel Multiplexers)

1 - What is the typical expected life (nb. of switches) of MOS comutations for
a typical application ?

1 - What is the typical expected life (nb. of switches) of MOS comutations for
a 30mA maximal continuous current (hot switching) ?

 

We don't specify this parameter. We do however, run the device for a length of
time , say 168 hours or 1000 hours at a high temperature, be it 85 deg or 125
deg, depending on the specification of the device. From this we calculate the
expected lifetime of the device.

Attachments

    Outcomes