ADG659: Supply voltage

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I'm planning to use the analog mux ADG659 in my circuit that has single 9 Vdc
supply. This component accept up to 13 V (maximum rating).The title of the
first page of the data sheet indicates: +3/+5/+-5V. In the Feature I read " 2V
to 12V single supply". I understand that this is compatible with my application
despite the title.


The ADG659 will work with the 9V single supply as long as the VSS pin is tied
to GND.
However, we have only characterized the device for 3V and 5V single supplies
and dual 5V supply which means that we cannot guarantee the performance
specified in the datasheet at 9V.