ADG453: Perfomance from +/- 15 V power supply

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I am considering the ADG453BR for a new design because of its low on
resistance. The objective is to use 2 SPST channels to make a DPST switch (by
connecting the outputs).  The signal inputs are TTL compatible and the signal
outputs are sent to a current feedback amplifier for amplification.

In a first instance, the signal frequency will be limited to 1 MHz but in
future applications, this signal should go up to 30MHz.

Is this a viable solution?

What kind of performance can I expect when the component is powered with a
single supply +12V (the datasheet only gives information on the frequency
response for +15,-15V and 50 ohm load)?


There will be very little difference between the On frequency response of the
ADG453 switch operating from a +/-15V supply and a 12V supply.  If you are not
concerned about the -1.5dB loss at 30MHz then this part should be a viable
solution for your application.