Radiation hardened/Space qualified parts

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Can you please let me know if there are Rad Hard versions of these parts?

ADG201HSTQ, ADG201HSTQ-ND
OP27GJZ, OP27GJZ-ND

 

Analog Devices offers radiation tolerant space qualified devices. Space
qualified devices are processed in accordance with the screening and quality
conformance inspection requirements of MIL-PRF-38535 for QML Class V devices. 
The radiation tolerance of the device is a separate issue that needs to be
evaluated by the program for suitability for a specific space level
application. Different space level applications have different radiation
tolerance requirements.

The following link contains a list of all space qualified parts from Analog
Devices:
http://www.analog.com/static/imported-files/aero_info/SpaceQualifiedPartsList.pd
f

The space qualified OP27S devices models are provided with Total Ionizing Dose
(TID) radiation inspection per MIL-STD-883 Test Method 1019 up to 100Krad. For
the part numbers kindly refer to the Space Qualified Parts list. For your
reference I copied the part numbers below:

OP27 - Low Noise Precision Op Amp
5962R9468002VGA (OP27AJ/QMLR)
5962R9468002VHA (OP27AL/QMLR)
5962R9468002V2A (OP27ARC/QMLR)
5962R9468002VPA (OP27AZ/QMLR)
5962L9468003VHA (OP27AL/QMLL).

Part 5962R9468002VGA (OP27AJ/QMLR) features the 8-lead TO-99 Can and
corresponds to the package type of OP27GJZ.

The space qualified ADG201-803Q devices are provided with no radiation
tolerance specification.  Customers who use this device perform their own
radiation inspection.  The typical TID radiation tolerance of the ADG201-803Q
devices is approximately 10 to 15Krad.
ADG201HS - LCMOS Hi-Speed QUAD SPST Switches
ADG201-803Q

The ADG201-803Q comes in a 16-lead Cerdip package (Package "Q").

Kindly also refer to the Space segment on our page
(http://mil-aero.analog.com/en/space/segment/ma.html) to find more information
regarding standards, packages, reports, etc.

Attachments

    Outcomes