Will the ADF7023 support spectrum inversion?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Does the ADF7023 support spectrum inversion?

 

The ADF7023 will generate FSK or GFSK, where the –Fdev is equivalent to a 0,
and the +FDev is equivalent to a 1, or OOK where the 0 is off, the 1 is on. If
by frequency inversion you want the opposite mapping of FDev, then this would
have to be done by inverting the source data.

The Tx test modes we offer are Tx carrier, Tx Preamble or Tx PN9, or SPORT Mode
Tx will simply follow the DataTransmit pin.

Attachments

    Outcomes