Confirm ADF4113HV has only two charge pump settings compared with the ADF4113?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Can you confirm that the ADF4113HV only has two charge pump current settings
compared to the ADF4113's 8 different settings (refer to page 17 of datasheet
Rev. D)?

 

Firstly, the ADF4113HV and ADF4113 may have similar names, but they are built
on two different technologies.
Yes, the ADF4113HV only has the two charge pump current settings. The charge
pump current can be adjusted via Rset.
The major difference between these devices is charge pump supply. The maximum
charge pump supply for the ADF4113 is 6V and for the ADF4113HV is 16.5V



1 person found this helpful

Attachments

    Outcomes