Q
required ADE7858 example source code & header files
A
use the common eval-board ADE78xx_eval_board_LPC2368_ver35_20081216.zipThe ADE7878 family of parts consist of the ADE7878, ADE7868, ADE7858 and
ADE7854. The EVAL-ADE7878EBZ can be used to evaluate all 4 parts without the
need of changing parts on the board
the project that was developed for the LPC2368 microcontroller that is
on the ADE7878 evaluation board.