ADE7878 load capacitors

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I want to check with us if I can use 30pF load capacitors with the crystal as
shown below in UG146 schematic. Is it required to use two 30 pF capacitors or
one would be sufficient?

 

The load capacitance of 30 pF is fine as far as the chip is the concerned.
However, the crystal manufacturer specifications also have to be checked for
load capacitance requirements. Also, when you are using a crystal, load
capacitances have to be used on both the pins-CLKIN and CLKOUT.

Attachments

    Outcomes