ADAU1761: Can I connect one analog and one digital input channel to the ADAU1761 and process both of them together?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

I need only left channel of SPDIF audio and  microphone in same time. It is
possible to configure codec to work in this way (analogue audio – MIC and  left
or right channel from digital input )? 

 

Yes, you can connect both one analog and one digital input channel to the
ADAU1761 and process both of them together. If you are using the serial digital
input port, you should ensure that the serial port is synchronized with the
master clock that is sent to the codec.

Attachments

    Outcomes