ADCMP343: Output response

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

My query is with how the device reacts on power up.

When the power to the device is ramping up below 1.7V, how does the output
respond?

I have used the ADCMP341 (non-inverting output) and the output tracks the power
rail and then for our set-up once a sufficient power level is reached, the
device switches low (the correct logic state).

How does the ADCMP343 (inverting) react during this 0 to 1.7V power up?

 

The application engineer has checked this on the bench here, and we can confirm
that the ADCMP343 output will be Hi-Z as the power supply rises up until it
starts to operate, at which point the output will depend on the state of the
inputs.

Attachments

    Outcomes