Reference Options

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

What are the reference options available for the ADAS3023?


The ADAS3023 allows using one of the three types of references as shown below.
• Internal, precision, low-drift 4.096V reference
• External 2.5V reference using the on-chip buffer
• External 4.096V reference with an external buffer