ADA4960-1 : Is there PSRR data available?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

Is there PSRR data for ADA4960-1, none is provided in the datasheet
specifications?

 

We do not normally specify PSRR for high speed amplifiers. There is no AC data
available but we do have DC data from the tester. According to the test data
for DC PSRR: the mean output-referred DC PSRR for
the positive supply is about 15 mV/V, or 36 dB, and for the negative supply it
is about 5 mV/V, or 46 dB.

Attachments

    Outcomes