This part is listed as a rail to rail input and output amplifier. How close to the supply rails does the ADA4807 swing?

Document created by analog-archivist Employee on Feb 23, 2016
Version 1Show Document
  • View in full screen mode

This part is listed as a rail to rail input and output amplifier. How close to
the supply rails does the ADA4807 swing?

 

The maximum allowable input range for the ADA4807 is 200mV below the negative
rail to 200mV above the positive rail for all supplies. The outputs will
typically swing to within 40mV of each rail. This value varies with respect to
supply.

Attachments

    Outcomes