Output Current

Document created by analog-archivist Employee on Feb 23, 2016Last modified by analog-archivist Employee on Feb 23, 2016
Version 2Show Document
  • View in full screen mode

How high of an output current can the ADA4661-2 and ADA4666-2 drive?

 

The ADA4661-2 and ADA4666-2 are capable of driving output currents up to 30 mA
with only 1V of dropout voltage. However, the usable output load current drive
is limited to the maximum power dissipation allowed by the device package used.
Always make sure not to exceed the maximum junction temperature (150OC) of the
device. To ensure proper operation, observe the following graph.

Attachments

Outcomes